Graphics Editor Libraries
When Graphics Editor is installed, a library of brushes, components, and snippets are included.
The brushes, components, and snippets are stored in:
C:\ProgramData\Schneider Electric\Power Operation\v2024\Applications\Graphics
Frequently used objects, animations, and behaviors are stored in the following sub folders:
Folder | Usage |
---|---|
\Brushes |
The Colors and Gradients palettes are stored here. |
\Components |
Standard symbols with specific meaning, and some other common symbols, are stored as components in the Components library, available in one of the window panes. A component can be dragged and dropped directly into the Design pane. New components can be added to the library. |
\Snippets |
A snippet is a piece of TGML code whose purpose is to store a “behavior” for reuse. A number of common behaviors are stored in the Snippets pane. A snippet can be dragged and dropped on an object in the Objects pane. Objects can be copied and modified, even created, and then saved as new snippets in the library. |
All subfolders in the Components library are displayed as clickable bars in the Components pane. All *.tgmlcomponent files in the Components subfolder are displayed as selectable components under the corresponding bar.
All subfolders in the Snippets library are displayed as clickable bars in the Snippets pane. All *.tgmlsnippet files in the Snippets subfolder are displayed as selectable snippets under the corresponding bar.